See the following figure for dimensions and physical features of
the WRZ-PTR0000-0 Series Temperature Sensor Probe assembly.
Figure 1. WRZ-PTR0000-0 Series Temperature Sensor Probe
assembly and dimensions, in. (mm)

| Callout | Description |
|---|---|
| A | 9 ft (2.7 m) wire lead |