Special tools needed - Johnson Controls - WRZ-PTR0000-0 - Wireless Device - WRZ-PTRxxxx-0 Series Temperature Sensor Probe
WRZ-PTR0000-0 Series Temperature Sensor Probe Assemblies Installation Guide
- Product
- Sensors and Meters > Room Sensor > WRZ-PTRxxxx-0 Series Temperature Sensor Probe
- Document type
- Installation Guide
- Document revision
- H
- Revision date
- 23/02/2023
- Part number
- 24-10332-29
- 1/16 in. (1.6 mm) Allen-head adjustment tool (Johnson Controls T-4000-119, order
separately) for the tamper-resistant set screw that secures the transmitter to the
mounting base
- Coin to unlock the transmitter housing from the mounting base locking tab