Special tools needed - Johnson Controls - WRZ-PTR0000-0 - Wireless Device - WRZ-PTR0000-0 Series Temperature Sensor Probe Assemblies

WRZ-PTR0000-0 Series Temperature Sensor Probe Assemblies Installation Guide

Brand
Johnson Controls
Product name
WRZ-PTR0000-0 Series Temperature Sensor Probe Assemblies
Document type
Installation Guide
Part number
24-10332-29
Document revision
G
Revision date
2020-07-09
Language
English
  • 1/16 in. (1.6 mm) Allen-head adjustment tool (Johnson Controls T-4000-119; order separately) for the tamper-resistant set screw that secures the transmitter to the mounting base
  • Coin to unlock the transmitter housing from the mounting base locking tab