Dimensions - Johnson Controls - LIT-12011640 - WRZ-7860-0 - Wireless Device - WRZ One-to-One wireless room sensing system

WRZ-7860-0 Receiver for One-to-One Wireless Room Sensing Systems Product Bulletin

Product
Document number
LIT-12011640
Revision date
2023-05-05
Product status
Discontinued

See the following figure for features and dimensions of the WRZ-7860-0 Receiver.

Figure 1. WRZ-7860-0 Receiver features and dimensions, in. (mm)

Callout Description
A Tamper-resistant set screw
B RJ-12 port for SA bus connection on the underside of the receiver
C Back of base to front of dome measurement
D Status LEDs