Dimensions - Johnson Controls - LIT-1900663 - WRZ-7860-0 - Wireless Sensor - WRZ-7860-0 Receiver for One-to-One Wireless Room Sensing System

WRZ-7860-0 Receiver for One-to-One Wireless Room Sensing Systems Catalog Page

Product
Sensors and Meters > Room Sensor > WRZ-7860-0 Receiver for One-to-One Wireless Room Sensing System
Document type
Catalog Page
Document number
LIT-1900663
Revision date
05/05/2023

See the following figure for features and dimensions of the WRZ-7860-0 Receiver.

Figure 1. WRZ-7860-0 Receiver features and dimensions, in. (mm)

Callout Description
A Tamper-resistant set screw
B RJ-12 port for SA bus connection on the underside of the receiver
C Back of base to front of dome measurement
D Status LEDs