Applications - Johnson Controls - LIT-1901179 - Wireless field bus - ZFR182x Pro Series Wireless Field Bus System - WNC1800 Wireless Network Coordinator Gateway

WRG1830/ZFR183x Pro Series Wireless Field Bus Coordinator Control Panel Assembly Catalog Page

Product
Network and Communications > Gateways and Routers > WNC1800 Wireless Network Coordinator Gateway
Document type
Catalog Page
Document number
LIT-1901179
Revision date
2023-06-16

The wireless products within a BAS system are ideal for any location where it is cost-prohibitive, difficult, or aesthetically unappealing to use a hard wire between BAS products. Examples of these locations include the following:

  • Office buildings, university campuses, educational facilities, correctional facilities, and other commercial structures with brick or solid concrete walls or ceilings, that impede hardwired applications.
  • Office buildings, retail stores, and other commercial real estate where tenant turnover is frequent and temporary walls and ceilings are common.
  • Museums, historical buildings, atriums, and other sites where building aesthetics and historical preservation are important.
  • Stadiums, arenas, gymnasiums, convention centers, airports, zoos, and other locations with large, open spaces with wood veneer, or other decorative surfaces that present challenges to hardwiring.
  • Buildings with asbestos or other hazardous materials that must not be disturbed.
  • Buildings with occupants sensitive to business disruptions.
  • Regions with high labor costs.

The WRG1830/ZFR183x Pro Series Wireless Field Bus System is approved by national compliance agencies for use in the United States and Canada. Refer to the WRG1830/ZFR183x Pro Series Wireless Field Bus System Catalog Page, LIT-1901153 for full technical specifications

Do not use the wireless BAS products in applications that cannot tolerate intermittent interference or where the following conditions apply:

  • Locations or applications that prohibit cellular telephones or Wi-Fi systems.
  • Critical control features would affect life safety or result in large monetary loss, including secondary (backup) life-safety applications.
  • Data centers, production lines, or critical areas would be shut down.
  • Loss of critical control would result from loss of data from humidity or temperature sensor communications.
  • Operation of exhaust fans or Air Handling Units (AHUs) would impair a purge or pressurization mode.
  • Missing data would invalidate reporting required by the customer.
  • Security points are monitored.