Most occupancy sensing NS Series Network Sensors have a default device address of 199 on the SA Bus. For the NS-MNN7003-0 model, the sensor address must be set on the dual-switch DIP switch block on the network sensor Printed Wire Board (PWB).
This addressable model is shipped with both switches set to ON, resulting in a device address of 203. Device addresses can be DIP switch set from 200 to 203; see Figure 3 and Table 1 for more details.
Figure 1. Dual-Switch DIP Switch Block (NS-MNN7003-0 Model)
DIP Switch Address | Switch 2 | Switch 1 |
---|---|---|
200 |
OFF |
OFF |
201 |
OFF |
ON |
202 |
ON |
OFF |
203 |
ON |
ON |