Overview - Johnson Controls - LIT-12013113 - NS8000 - Network sensor - NS8000 Series Network Sensor

Vertical Wallbox-Mounted or Surface-Mounted NS8000 Series Network Sensors Product Bulletin

Product
Sensors and Meters > Network Sensors > NS8000 Series Network Sensor
Document number
LIT-12013113
Revision date
2024-09-17
Figure 1. LCD full color graphical display, LCD fixed segment display, Warmer/Cooler interface, No display

The NS8000 Series Network Sensors function directly with Metasys system Field Equipment Controllers (FECs), Metasys Network and Control Engines (NCEs), Advanced Application Field Equipment Controller (FACs), Metasys VAV Box Equipment Controllers (CVM), General Purpose Application Controllers (CGM), VAV Modular Assembly (VMA16) Controllers, and Facility Explorer FX-PC Series Programmable Controllers (FX-PCGs, FX-PCVs, and FXPCXs). The sensors are also compatible with Verasys and Johnson Controls® Smart Equipment.

The NS8000 Series Network Sensors monitor zone temperature, relative humidity (RH), carbon dioxide (CO2 ), motion, and local temperature setpoint adjustments. The sensor transmits this data to a controller on the Sensor Actuator (SA) bus.

Some NS8000 Series Network Sensors models include an onboard passive infrared (PIR) occupancy sensor that detects motion to determine if a space is occupied. This feature maximizes up to 30% energy savings in high-energy usage environments such as schools, dormitories, offices, hospitals, and hotels by adjusting the temperature of the space based on the occupancy status. In addition, the PIR occupancy sensor facilitates trending of floor space usage in these environments.

Display models of the NS8000 Series Network Sensors are available with a backlit LCD fixed segment display or a full color graphical LCD interface. These models allow the user to view zone temperature, RH, CO2, and adjust the zone temperature setpoint and fan speed. Graphical models provide a summary of sensor values at the base of the display. Fixed segment models have the capability to set the default display to temperature, RH, or temperature setpoint.

The user can also choose between degrees Fahrenheit (F) and degrees Celsius (C). To prevent tampering with the sensor, display models also include a screen lockout feature. The graphical display enables the user to choose between a light or dark color theme and to set the sleep mode to dim or turn off.

Some models also have a Warmer/Cooler interface to adjust the zone temperature. Instead of a display, these models have two cap touch buttons with seven LED lights that represent the current setpoint. The display models include the following fan speeds: automatic, off, low, medium, or high.

Interaction with the sensor sets the occupancy override function to signal to the controller that the zone is occupied and to override the scheduled mode. The LCD full color graphical models use the graphical user interface to set a unique BACnet® address for applications that require multiple sensors. Other models have DIP switches to set a unique address for applications that require multiple sensors. All models ship standard with modular phone jacks and screw terminals to terminate the wiring connecting the sensors to the controller.

Note: To connect the NS8000 Series Network Sensor to the same SA bus segment, use only one of the two connection methods, either the modular phone jack or the screw terminals.

Each network sensor includes a SA bus access port, allowing for accessories to connect to the SA bus. Through this connector, the user can use accessories to service or commission the connected controller or gain access to any other controller on the same field controller (FC) bus.

Note: Device programming for the NS8000 sensor connected to the controller does not include balancing functionality and features.

The NS8000 Series Network Sensors can be surface-mounted or vertical wallbox-mounted to meet the requirements of the specific application. All display models are optimized for the California Energy Code (Title 24).

Modern enclosures in a white design are available in the following styles:

  • LCD fixed segment display and LCD full color graphical display: View zone temperature, RH, CO2, occupancy status, and adjust the zone temperature setpoint and fan speed. These models have the capability to set the default display to temperature, RH or temperature setpoint. On these display models, you can also choose between degrees Fahrenheit (F) and degrees Celsius (C).
  • Warmer/Cooler interface: This interface incorporates cap touch buttons with seven LED lights that represent the current setpoint status.
  • No display: The NS8000 Series Network Sensors are available in a high gloss white finish with or without the Johnson Controls logo.
  • All sensors are serialized for quality and warranty purposes. Based on the serial number, the user can obtain a certificate of conformance.

See Table 1 through Table 6 for ordering information.