Ordering information - Johnson Controls - LIT-12013113 - NS8000 - Network sensor - NS8000 Series Network Sensor

Vertical Wallbox-Mounted or Surface-Mounted NS8000 Series Network Sensors Product Bulletin

Product
Sensors and Meters > Network Sensors > NS8000 Series Network Sensor
Document type
Product Bulletin
Document number
LIT-12013113
Revision date
2024-09-17

See Table 1 through Table 6 for the various NS8000 Series Network Sensor models available. See Table 7 for accessories.

Note: Product codes marked with an asterisk are made in America to meet the Buy American Standard.
Important: The NS8000 Series Network Sensor is intended to provide an input to equipment under normal operating conditions. Where failure or malfunction of the network sensor could lead to personal injury or property damage to the controlled equipment or other property, additional precautions must be designed into the control system. Incorporate and maintain other devices, such as supervisory or alarm systems or safety or limit controls, intended to warn of or protect against failure or malfunction of the network sensor.
Note: Keep the Metasys system software up to date as some NS8000 Series Network Sensor features are not supported in previous releases of Metasys, Facility Explorer, Verasys, or Johnson Controls Smart Equipment system software.