Temperature/RH Mode Selection - Johnson Controls - Part No. 24-10094-25 - Vertical Wallbox-Mounted or Surface-Mounted NS Series Network Sensors with LCD

Vertical Wallbox-Mounted or Surface-Mounted NS Series Network Sensors with LCD Installation Guide

Product
Sensors and Meters > Network Sensors > Vertical Wallbox-Mounted or Surface-Mounted NS Series Network Sensors with LCD
Document number
Part No. 24-10094-25
Document revision
P
Revision date
2021-03-31

About this task

Temperature/RH models include an RH% pushbutton on the face of the network sensor to allow occupants to view the temperature and relative humidity of the zone. Press the RH% pushbutton to toggle between temperature and RH% on the LCD. The LCD defaults to temperature 5 seconds after the RH% pushbutton is released.

The NS-BHR710x-0 models also have the capability to set the default display to either temperature or RH%. Follow this procedure to change the default display on these models:

Procedure

  1. If the display backlight is off, press and release the RH% pushbutton to illuminate the backlight. If the display backlight is already on, proceed to Step 2.
  2. Press and hold the RH% pushbutton for 5 seconds to switch to a different default display (either temperature or RH%).
    Note: The default display flashes for 5 seconds. After the display stops flashing, the new default display is in effect.
  3. Release the RH% pushbutton; the display that you selected is now the new default display.