About this task
Temperature/RH models include an RH% pushbutton on the face of the network sensor to allow occupants to view the temperature and relative humidity of the zone. Press the RH% pushbutton to toggle between temperature and RH% on the LCD. The LCD defaults to temperature 5 seconds after the RH% pushbutton is released.
The NS-BHR710x-0 models also have the capability to set the default display to either temperature or RH%. Follow this procedure to change the default display on these models: