Temperature Setpoint Adjustment/Occupancy Override - Johnson Controls - Part No. 24-10094-25 - Vertical Wallbox-Mounted or Surface-Mounted NS Series Network Sensors with LCD

Vertical Wallbox-Mounted or Surface-Mounted NS Series Network Sensors with LCD Installation Guide

Product
Sensors and Meters > Network Sensors > Vertical Wallbox-Mounted or Surface-Mounted NS Series Network Sensors with LCD
Document number
Part No. 24-10094-25
Document revision
P
Revision date
2021-03-31

You can use either the large dial or the pushbuttons on the face of the network sensor to change the controller mode from unoccupied to occupied, or to adjust the temperature setpoint.

To change the occupancy mode using the dial, rotate the dial slightly, so the backlight on the LCD lights up. If you rotate the dial slightly again, and the controller is in the unoccupied mode, the controller changes from the after-normal-working-hours setback mode to the normal-working-hours comfort mode. Alternatively, you can use the pushbuttons to change the controller mode from unoccupied to occupied.

To adjust the setpoint using the dial, continue rotating the dial until the current setpoint is displayed and flashing. Turn the dial clockwise to increase the setpoint and counterclockwise to decrease the setpoint. Stop turning the dial once the preferred setpoint is reached. The new setpoint stops flashing and becomes fixed after a few seconds. To use the pushbuttons instead, press the up arrow button to increase the setpoint or the down arrow to decrease it.