Network Sensor Addressing - Johnson Controls - Part No. 24-10094-25 - Vertical Wallbox-Mounted or Surface-Mounted NS Series Network Sensors with LCD

Vertical Wallbox-Mounted or Surface-Mounted NS Series Network Sensors with LCD Installation Guide

Product
Sensors and Meters > Network Sensors > Vertical Wallbox-Mounted or Surface-Mounted NS Series Network Sensors with LCD
Document number
Part No. 24-10094-25
Document revision
P
Revision date
2021-03-31

Most network sensors have a default device address of 199 on the SA Bus. For the NS-BTB7003-0 addressable model, the sensor address must be set on the dual-switch DIP switch block on the network sensor Printed Wire Board (PWB).

The averaging model is shipped with both switches set to ON, resulting in a device address of 203. Device addresses can be DIP switch set from 200 to 203; see Figure 4 and Table 1 for more details.

Figure 1. Dual-SwitchDIP Switch Block

Table 1. Network Sensor Addressing
DIP Switch Address Switch 2 Switch 1
200 OFF OFF
201 OFF ON
202 ON OFF
203 ON ON