Most network sensors have a default device address of 199 on the SA Bus. For the NS-BTB7003-0 addressable model, the sensor address must be set on the dual-switch DIP switch block on the network sensor Printed Wire Board (PWB).
The averaging model is shipped with both switches set to ON, resulting in a device address of 203. Device addresses can be DIP switch set from 200 to 203; see Figure 4 and Table 1 for more details.
Figure 1. Dual-SwitchDIP Switch Block
DIP Switch Address | Switch 2 | Switch 1 |
---|---|---|
200 | OFF | OFF |
201 | OFF | ON |
202 | ON | OFF |
203 | ON | ON |