Fan Mode Selection - Johnson Controls - Part No. 24-10094-25 - Vertical Wallbox-Mounted or Surface-Mounted NS Series Network Sensors with LCD

Vertical Wallbox-Mounted or Surface-Mounted NS Series Network Sensors with LCD Installation Guide

Product
Sensors and Meters > Network Sensors > Vertical Wallbox-Mounted or Surface-Mounted NS Series Network Sensors with LCD
Document number
Part No. 24-10094-25
Document revision
P
Revision date
2021-03-31

Some models include a fan mode pushbutton on the face of the network sensor to select the desired fan speed. Pressing the pushbutton toggles the fan speed between AUTO-OFF-LOW-MEDIUM-HIGH on the LCD.