Repair Information - Johnson Controls - Part No. 24-10094-25 - Vertical Wallbox-Mounted or Surface-Mounted NS Series Network Sensors with LCD

Vertical Wallbox-Mounted or Surface-Mounted NS Series Network Sensors with LCD Installation Guide

Product
Sensors and Meters > Network Sensors > Vertical Wallbox-Mounted or Surface-Mounted NS Series Network Sensors with LCD
Document type
Installation Guide
Document number
Part No. 24-10094-25
Document revision
P
Revision date
2021-03-31

If the NS Series Network Sensor fails to operate within its specifications, replace the unit. For a replacement network sensor, contact the nearest Johnson Controls representative.