The non-permanent values can be set and cleared with the UVM Configuration Tool. The UVM reacts to their selections. If loss of power occurs, these settings do not retain their selected state when power is re-applied. When starting the device, the values are inactive or not checked.
The override AO 1 (VO) setting disconnects the Vo output from the control logic. The override AO 1 (VO) enables the user to set a VO control value directly. The control operate through the feedback output field and set feedback output raw value button on the dynamic values tab.
- Click the Override AO 1 (Vo) check box and click the Dynamic Values tab.
- In the FeedBack Output field, enter a value between 0 CFM and 1000 CFM, where 0 is 0 volts and 1000 is 10 volts.
- Click the Set Feedback Output Raw Value button to write the value to the AO 1 (VO) signal.
The override AO 2 (Act) setting disconnects the actuator Io output from the control logic and enables the user to control the IO directly. The control operates through the actuator output field and the set actuator raw output Value button on the dynamic values tab.
- Check the Override AO 2 (Io) check box and click the Dynamic Values tab.
- Enter a value between 0 CFM and 1000 CFM, where 0 is 4 mA (0%) and 1000 is 20 mA (100%), in the Actuator Output field.
- Click the Set Actuator Output Raw Value button to write the value to the AO 2 (IO) signal.