OEM voltage to CFM entry - Johnson Controls - LIT-12014272 - Valve - Venturi Valve

Venturi Air Valve with UVM1000 Installation Guide

Brand
Johnson Controls
Product name
Venturi Valve
Document type
Installation Guide
Document number
LIT-12014272
Revision date
2023-03-10
Language
English

To enter the OEM voltage to CFM entry, see the following steps:

  1. From lowest value to highest value, enter the minimum and maximum CFM values and the minimum and maximum voltages from the valve label.
  2. To automatically enter the position and CFM values into the table on the main screen, click the Compute button.
  3. When finished, click Close the OEM Voltage dialog box.