The dynamic values tab provides a set of buttons and fields to access dynamic values within the controller.
The tab finds faults and debugs performance issues. Output override values can also be set from here. If selected, you can enter a soft setpoint.
The values displayed include calculated values such as CFM, position, and pressure. Also displayed are raw A/D values from the AI inputs. The values do not automatically update. To read a value, click the associated value button.