You can use the user settings tab to configure settings for the UVM. The settings that are available on the tab depend on the mode of operation and the options that are available for that mode.
To load specific information onto the controller, use the individual set buttons.
Note: Do not overwrite the factory calibration values in the
UVM for the AO and AI ports.