Module calibration information - Johnson Controls - LIT-12014272 - Valve - Venturi Valve

Venturi Air Valve with UVM1000 Installation Guide

Product
Valves and Actuators > Valves > Venturi Valve
Document number
LIT-12014272
Revision date
2023-03-10
The factory uses module calibration information for setup of the UVM. The field enables the importation of the valve curves and valve data for inclusion in the UVM storage. The field also creates valve summary labels. You can calibrate the feedback sensor from the CFM Table tab.
Note: Do not use this field unless under instruction from Triatek.