Internal configuration settings - Johnson Controls - LIT-12014272 - Valve - Venturi Valve

Venturi Air Valve with UVM1000 Installation Guide

Brand
Johnson Controls
Product name
Venturi Valve
Document type
Installation Guide
Document number
LIT-12014272
Revision date
2023-03-10
Language
English
The factory programs and calibrates the AI and AO channels with the fields in the Internal Configuration settings tab. The tab contains the gain and offset settings for each of the channels.
Note: Do not adjust these values unless instructed by Triatek.

The entries show a factory calibration value and an acceptable range for the value. If the value is within range, it has a yellow background. If the value is out of range, it has a red background.

The user can adjust the ranges to correct any voltage errors that occur. Refer to Procedure to Check I_O on a UVM Board for more information.

The factory uses the auto calibrate button to automatically adjust the gain and offset values for the analog channels while calibration occurs. This process requires specialized test equipment to operate correctly.