UVM Configuration Tool - Johnson Controls - LIT-12014272 - Valve - Venturi Valve

Venturi Air Valve with UVM1000 Installation Guide

Brand
Johnson Controls
Product name
Venturi Valve
Document type
Installation Guide
Document number
LIT-12014272
Revision date
2023-03-10
Language
English

Before you begin

To set up the UVM configuration tool, see the following steps:

Procedure

  1. Download the UVM1000 configuration software (ValveLinModuleLabeler.exe) from the Johnson Controls License Portal onto the UVM configuration tool.
  2. Install Microsoft Visual Basic (VB) Powerpack 10 to initiate the UVM Configuration Tool. Use the following link to install the Microsoft VB Powerpack manually: http://go.microsoft.com/fwlink/?LinkID=145727&clcid=0x804.
  3. Use a USB to DB9 cable to connect the mounted UVM1000 to the Venturi air valve. For the cable part number, see Figure 23.