Introduction - Johnson Controls - LIT-12014272 - Valve - Venturi Valve

Venturi Air Valve with UVM1000 Installation Guide

Product
Valves and Actuators > Valves > Venturi Valve
Document number
LIT-12014272
Revision date
2023-03-10

The Universal Valve Module is designed to enable interoperability between Venturi valves and third party controllers.

Each Venturi valve is individually characterized on a calibrated air line at the factory to generate its own unique position to cubic feet per minute (CFM) curve. You can use the UVM to create a linearization curve in each UVM1000 module for each associated valve. The linearization curve is accesible through 0 VDC to 10 VDC command control signal. You can also use the UVM to span, scale, and linearize the feedback sensor to obtain useful information from UVM.