VG1000 Series Ball Valves are designed to regulate the flow of hot or chilled water and, for some models, low-pressure steam in response to the demand of a controller in HVAC systems. Available in sizes 1/2 through 1 in. (DN15 through DN25), this family of two and three-way forged brass valves is factory or field mounted to Johnson Controls ® VA9104 Series Non-Spring-Return and VA9203 Series Spring-Return Electric Actuators for on/off, floating, or proportional control. When supplied with an actuator, the actuator is not mounted to the valve to allow access to the end connections.
Refer to the VG1000 Series Forged Brass Ball Valves Product Bulletin (LIT-977132) for important product application information.