Network Security Options - Johnson Controls - LIT-12013604 - JC-VAV1507-0 - Variable air volume controller - VAV1507 Modular Assembly

VAV1507 VAV Controller BACnet Protocol Implementation Conformance Statement

Product
Variable Air Volume > Modular Assemblies > VAV1507 Modular Assembly
Document number
LIT-12013604
Revision date
2025-01-21
Product status
Active
Non-secure Device - is capable of operating without BACnet Network Security
Secure Device - is capable of using BACnet Network Security (NS-SD BIBB)
  Multiple Application-Specific Keys:
  Supports encryption (NS-ED BIBB)
  Key Server (NS-KS BIBB)