This document contains the Protocol Implementation Conformance Statement (PICS) and BACnet® Interoperability Building Blocks (BIBBs) for the VAV1507 VAV Controller, JC-VAV1507-0, as required by the ANSI/ASHRAE® Standard 135 for BACnet protocol.
The PICS is a written document created by the manufacturer of a device to identify the particular options specified in the BACnet standard and implemented in the device.
BIBBs are collections of one or more BACnet services. This document includes a listing of the BIBBs currently supported by the VAV1507.