Document Introduction - Johnson Controls - LIT-12013604 - JC-VAV1507-0 - Variable air volume controller - VAV1507 Modular Assembly

VAV1507 VAV Controller BACnet Protocol Implementation Conformance Statement

Brand
Johnson Controls
Product name
VAV1507 Modular Assembly
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013604
Revision date
2020-08-13
Product status
Active
Language
English

This document contains the Protocol Implementation Conformance Statement (PICS) and BACnet® Interoperability Building Blocks (BIBBs) for the VAV1507 VAV Controller, JC-VAV1507-0, as required by the ANSI/ASHRAE® Standard 135 for BACnet protocol.

The PICS is a written document created by the manufacturer of a device to identify the particular options specified in the BACnet standard and implemented in the device.

BIBBs are collections of one or more BACnet services. This document includes a listing of the BIBBs currently supported by the VAV1507.