BACnet Interoperability Building Blocks (BIBBs) (Annex K) - Johnson Controls - LIT-12013604 - JC-VAV1507-0 - Variable air volume controller - VAV1507 Modular Assembly

VAV1507 VAV Controller BACnet Protocol Implementation Conformance Statement

Product
Variable Air Volume > Modular Assemblies > VAV1507 Modular Assembly
Document number
LIT-12013604
Revision date
2025-01-21
Product status
Active

The following table lists all BIBBs that are supported. The table is divided into BIBBs required for the Controller (B-ASC) profile, followed by additional BIBBs that are supported, but not required, for the profile.

Table 1. BACnet B-ASC BIBBs Support

BIBB Name (A = Initiates and B = Executes)

Designation

Required for the B-ASC profile

Data Sharing - Read Property - B

DS-RP-B

Data Sharing - Write Property - B

DS-WP-B

Device Management - Dynamic Device Binding - B

DM-DDB-B

Device Management - Dynamic Object Binding - B

DM-DOB-B

Device Management - Device Communication Control - B

DM-DCC-B

Not required for the B-ASC profile

Data Sharing - Read Property - A

DS-RP-A

Data Sharing - Read Property Multiple - B

DS-RPM-B

Data Sharing - Write Property - A

DS-WP-A

Data Sharing - Write Property Multiple - B

DS-WPM-B

Data Sharing - Change Of Value - B DS-COV-B
Data Sharing - Change Of Value Property - B DS-COVP-B

Data Sharing - Change Of Value Unsubscribed - B

DS-COVU-B

Executes ReadRange Executes ReadRange

Device Management - Dynamic Device Binding - A

DM-DDB-A

Device Management - Time Synchronization - B

DM-TS-B

Device Management - UTC Time Synchronization - B

DM-UTC-B

Device Management - Reinitialize Device - B

DM-RD-B

Device Management - Restart - B

DM-R-B

Device Management - List Manipulation - B DM-LM-B