Description - Johnson Controls - LIT-1924095 - Accessories - V-9000-500 Positioner

V-9000-500 Positioner Catalog Page

Product
Valves and Actuators > Positioners > V-9000-500 Positioner
Document type
Catalog Page
Document number
LIT-1924095
Revision date
2019-10-08
Figure 1. V-9000-500 Positioner

Use the V-9000-500 Positioner for modulating control of both double-acting and spring-return actuators.

When the V-9000 Series Rack and Pinion Actuator is ordered as a factory-mounted component of a complete VF Series Butterfly Valve assembly, the positioner can be ordered as a factory-installed option.

Specify code number V-9000-500 when ordering; the appropriate mounting kit must be ordered separately.

Refer to the V-9000 Series Rotary Motion Rack and Pinion Pneumatic Actuators for Butterfly Valves Product Bulletin (LIT-977260) for important product application information (including mounting kits).