Features - Johnson Controls - LIT-1924055 - Pneumatic Actuator - V-3000 Series Pneumatic Actuator

V-3000 Series Pneumatic Actuator Catalog Page

Product
Valves and Actuators > Pneumatic Actuators > V-3000 Series Pneumatic Actuator
Document type
Catalog Page
Document number
LIT-1924055
Revision date
2019-10-01
  • Molded synthetic rubber diaphragm design provides a constant effective area throughout the valve stem stroke
  • Die-cast aluminum housing coated with corrosion-resistant finish
  • Remove or reposition actuator by loosening a single set screw
  • Easily field mounted to the valve bonnet with a single set screw
  • Can be mounted to any of the V-3000,V-4000, or VT Series Valves (except V-3854)