Ventilator accessory control - Johnson Controls - S1-SE-CUA1001-0 - Universal Adapter

Universal Adapter Installation Guide

Product
Accessories > Adapters > Universal Adapter
Document type
Installation Guide
Document revision
B
Revision date
2021-07-28
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-02198

The UA can command a ventilator accessory board.

Use the ventilator-related parameters in the Settings menu to configure the ventilation device type and operation.