Float switch for the AVV air handler or a two-stage furnace - Johnson Controls - S1-SE-CUA1001-0 - Universal Adapter

Universal Adapter Installation Guide

Product
Accessories > Adapters > Universal Adapter
Document type
Installation Guide
Document revision
B
Revision date
2021-07-28
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-02198

When the UA connects to the AVV air handler or a two-stage furnace, you can configure the UA to monitor the indoor control’s float switch input.

When the float switch activates, the UA disables compressor operation for five minutes. If the float switch is still active after the five minutes, the UA continues to disable compressor operation until the float switch deactivates.

You can configure the float switch operation with the Settings > Float Switch parameter in the following way:

  • Disabled: the UA does not affect compressor operation based on float switch behavior.
  • Enabled Open: if the float switch is open, the UA suspends compressor operation for at least five minutes.
  • Enabled Close: if the float switch is closed, the UA suspends compressor operation for at least five minutes.