Sequence of operation - Johnson Controls - S1-SE-CUA1001-0 - Universal Adapter

Universal Adapter Installation Guide

Product
Accessories > Adapters > Universal Adapter
Document revision
B
Revision date
2021-07-28
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-02198

On startup, the UA attempts to communicate with all possible connected devices. When a compatible device is connected and responds, the UA indicates that device as online and establishes communication with it.