Setup overview - Johnson Controls - S1-SE-CUA1001-0 - Universal Adapter

Universal Adapter Installation Guide

Product
Accessories > Adapters > Universal Adapter
Document revision
B
Revision date
2021-07-28
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-02198

To set up your Universal Adapter, perform the following steps:

  1. Mount and wire the adapter according to the Installation section.
  2. Configure the adapter using the local display or the Mobile Access Portal (MAP) Gateway. For the available menu options, see Configuration. For detailed information about how the adapter operates, see Sequence of operation.