Using the local LCD - Johnson Controls - S1-SE-CUA1001-0 - Universal Adapter

Universal Adapter Installation Guide

Product
Accessories > Adapters > Universal Adapter
Document revision
B
Revision date
2021-07-28
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-02198

Use the push buttons next to the LCD to navigate the menu and modify properties in the following way:

  • To move the cursor, press the up and down arrow buttons.
  • To select a menu item, press the Ent button.
  • To modify the value of a property, press the Ent button to select the property, and then press the up and down arrow buttons to select a new value.
  • To go back to the previous item, press the Esc button.