| Level 2 | Description | Available values |
|---|---|---|
| View Version | Displays the current firmware version and status. | n/a |
| Load Firmware | If you insert a USB drive into the USB port of the adapter, you can select a firmware package file to load. | n/a |
| Backup | You can create a backup of the device. |
Backup: Wait, Backup 0% Backup: Ok, Backup 100% |
| Restore | You can restore data from a backup file. |
BackupConfig (file name to be restored) |