System menu - Johnson Controls - S1-SE-CUA1001-0 - Universal Adapter

Universal Adapter Installation Guide

Product
Accessories > Adapters > Universal Adapter
Document revision
B
Revision date
2021-07-28
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-02198
Note: A submenu appears only if the relevant control is connected to the adapter.
Table 1. System > Variable Capacity menu
Name Description
Outdoor Temp Displays the outdoor temperature sensor reading from the variable capacity control.
W1 Output Displays the status of the variable capacity control’s W1 output.
Note: This item appears only when its status is on.
W2 Output Displays the status of the variable capacity control’s W2 output.
Note: This item appears only when its status is on.
HP Lockout Displays the status of the variable capacity control’s heat pump lockout.
Note: This item appears only when its status is on.
Aux Lockout Displays the status of the variable capacity control’s auxiliary heat lockout.
Note: This item appears only when its status is on.
Table 2. System > Modulating Furnace menu
Name Description
Indoor CFM Displays the blower flow rate for the modulating furnace control.
HUM Output Displays the status of the modulating furnace control’s humidifier output.
Note: This item appears only when its status is on.
EAC Output Displays the status of the modulating furnace control’s electric air cleaner output.
Note: This item appears only when its status is on.
Table 3. System > AVV Air Handler menu
Name Description
Indoor CFM Displays the blower flow rate for the AVV air handler control.
FLT SWT Input Displays the status of the AVV air handler control’s float switch input.
Note: This item appears only when its status is on.
EAC Output Displays the status of the AVV air handler control’s electric air cleaner output.
Note: This item appears only when its status is on.
HUM Output Displays the status of the AVV air handler control’s humidifier output.
Note: This item appears only when its status is on.
Table 4. System > 2 Stage Furnace menu
Name Description
Indoor CFM Displays the blower flow rate for the two-stage furnace control.
FLT SWT Input Displays the status of the two-stage furnace control’s float switch input.
Note: This item appears only when its status is on.
UTIL Input Displays the status of the two-stage furnace control’s auxiliary switch input.
Note: This item appears only when its status is on.
HUM Output Displays the status of the two-stage furnace control’s humidifier output.
Note: This item appears only when its status is on.
EAC Output Displays the status of the two-stage furnace control’s electric air cleaner output.
Note: This item appears only when its status is on.