Status menu - Johnson Controls - S1-SE-CUA1001-0 - Universal Adapter

Universal Adapter Installation Guide

Product
Accessories > Adapters > Universal Adapter
Document revision
B
Revision date
2021-07-28
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-02198
Table 1. Status menu
Name Description
Y1 Displays the on or off status of the incoming signal from the thermostat.
Note: An item appears only when its status is on.
Y2
W1
W2
G
O
AI1 Sensor Displays the temperature measurement from the AI sensors.
Note: An item appears only if you connect a sensor to the relevant AI. If a sensor disconnects during operation, the item still appears until the next power cycle of the adapter.
AI2 Sensor
AI Average Displays the effective temperature measurement based on the AI1 and AI2 measurements.