The following table lists the alarms that can appear for the adapter.
Note: In the MAP
Gateway user interface, alarm times may be missing, because the adapter does not
contain a clock.
Name | Description |
---|---|
OD Comm Fault | The UA has lost communication with the outdoor control for longer than 10 seconds. |
ID Comm Fault | The UA has lost communication with the indoor control for longer than 10 seconds. |
Modbus Comm Err | The UA can communicate with the control, but an error occurred in the Modbus communication. |
OD Equip Fault | The outdoor control is experiencing a fault. See the outdoor control for details. |
ID Equip Fault | The indoor control is experiencing a fault. See the indoor control for details. |
Vent Fault | The ventilator accessory control is experiencing a fault. See the ventilator accessory control for details. |
No Temp Sensor | The alarm appears if you set | to 1, but no sensor is connected to AI1 or AI2.
No AI1 Sensor | The alarm appears if you set | to 2, but no sensor is connected to AI1.
No AI2 Sensor | The alarm appears if you set | to 2, but no sensor is connected to AI2.