Remapping Points - Johnson Controls - LIT-12012523 - Temperature Data Acquisition Module

Temperature Data Acquisition (TDA) Module Technical Bulletin

Product
Building Automation Systems > Databases and Data Servers > Temperature Data Acquisition Module
Document number
LIT-12012523
Revision date
2021-03-30

To remap a TDA Module to an NAE at the same FC bus address, select the displayed field points individually in the Point Mapping Utility. There are 41 field points that can be selected.