Adding a TDA Module - Johnson Controls - LIT-12012523 - Temperature Data Acquisition Module

Temperature Data Acquisition (TDA) Module Technical Bulletin

Product
Building Automation Systems > Databases and Data Servers > Temperature Data Acquisition Module
Document type
Installation Guide
Document number
LIT-12012523
Revision date
2021-03-30

The TDA Module must be added before its points can be mapped. To add the TDA Module, select the Field Bus and choose Field Device from the Insert menu.

Assisted Definition using Auto Discovery is the easiest way to add a new TDA Module online; however, this method requires that the TDA Module to be added is connected and ready to communicate. Device addresses must be unique from 4-127.