Adding BACnet MS/TP Points - Johnson Controls - LIT-12012523 - Temperature Data Acquisition Module

Temperature Data Acquisition (TDA) Module Technical Bulletin

Product
Building Automation Systems > Databases and Data Servers > Temperature Data Acquisition Module
Document type
Installation Guide
Document number
LIT-12012523
Revision date
2021-03-30

The required points must be mapped under the TDA Module. To map the points, select the TDA Module device under the BACnet Integration and choose Field Point from the Insert menu. If necessary, refresh the tree view to see a newly added TDA Module. Refer to Table 2 for a list of supported points on the TDA Module.

When mapping points offline, the point type must match the BACnet object type (for example, AI, AV, MV, or BO) and the point instance number must match the BACnet instance number.