Recommended System Configuration Practices - Johnson Controls - LIT-12012523 - Temperature Data Acquisition Module

Temperature Data Acquisition (TDA) Module Technical Bulletin

Product
Building Automation Systems > Databases and Data Servers > Temperature Data Acquisition Module
Document number
LIT-12012523
Revision date
2021-03-30

When connected to a BAS, there may be a need to limit command and view access to configuration parameters. This can be done through proper configuration of user access settings within the BAS. In the case of theJohnson Controls NAE, refer to Security Administrator System Technical Bulletin Code (LIT-1201528).