Description - Johnson Controls - LIT-1900058 - Humidity Sensor - TRUERH Humidity Controllers

TRUERH Humidity Controllers Catalog Page

Product
Controls > Humidity Controls > TRUERH Humidity Controllers
Document type
Catalog Page
Document number
LIT-1900058
Revision date
2020-02-19

The HC-67x3 Series TrueRH™ Humidity Controllers come in both wall or duct mount packages. These attractively styled controllers offer ease of installation and application flexibility. The patented All-Polymer™ humidity sensor construction improves resistance to chemical corrosion.

The HC-67x3 functions as a proportional humidity controller.

The output is jumper-selectable Reverse Acting (RA) or Direct Acting (DA), along with an adjustable setpoint and proportional band.

Refer to the HC-67x3 Series TrueRH Humidity Controllers Product Bulletin (LIT-216265) for important product application information.

Figure 1. HC-6703-4N00W Wall Mount Humidity Controller

Figure 2. HC-6703-6N00P Duct Probe Humidity Controller