Applications to avoid using wireless - Johnson Controls - LIT-12013954 - JC-TMR2400-x - Wireless Device - TMR Series Wireless Best Practices

TMR Series Wireless Best Practices

Product
Network and Communications > Wireless Devices > TMR Series Wireless Best Practices
Document type
Commissioning Guide
Document number
LIT-12013954
Revision date
2022-09-01

Do not use the wireless products in applications that do not allow wireless devices or cannot tolerate intermittent data loss. Examples include the following:

  • Many government buildings do not allow any wireless devices. For example, Department of Defense.
  • Critical control applications that could affect life safety or result in large monetary loss, including secondary (backup) life-safety applications.
  • Data centers, production lines, or critical areas would be shut down.
  • Missing data would invalidate reporting required by the customer security points are monitored.