User lockout - Johnson Controls - TEC3022-1x-xxx - TEC3023-1x-xxx - TEC312x-14-xxx - TEC3322-1x-xxx - TEC3323-1x-xxx - TEC3622-1x-xxx - TEC3623-1x-xxx - Proportional Fan Coil Thermostat - Thermostats - TEC3000 Series Networked and Wireless Proportional Fan Coil and Individual Zone thermostats with Dehumidification Capability

TEC3000 Series Proportional Fan Coil Thermostats Quick Start Guide

Product name
TEC3000 Series Networked and Wireless Proportional Fan Coil and Individual Zone thermostats with Dehumidification Capability
Document type
Quick Start Guide
Document revision
G
Revision date
2024-03-08
docpartnumberlabel
Part No.
Part number
24-11353-00028

You can select from three different levels of access at the local display to manage functionality through the supervisory controller. This lockout is independent of any display or passcode settings. The existing temporary occupancy capability is unaffected by this feature. User lockout hides the icons that are not operable. The lockout levels are described in Table 1.

Table 1. User lockout levels
Lockout level Capability
State 0 Provides full access to Home Screen Display Adjustments and icons (default).
State 1 Hides the Menu icon.
State 2 Only allows the screen to trigger temporary occupancy. Menu, Unit Power, the Up and Down arrows, and Run/Hold are hidden.