Touchscreen icons - Johnson Controls - TEC312x-14-xxx - TEC3023-1x-xxx - TEC3322-1x-xxx - TEC3622-1x-xxx - TEC3022-1x-xxx - TEC3623-1x-xxx - TEC3323-1x-xxx - Proportional Fan Coil Thermostat - Thermostats - TEC3000 Series Networked and Wireless Proportional Fan Coil and Individual Zone thermostats with Dehumidification Capability

TEC3000 Series Proportional Fan Coil Thermostats Quick Start Guide

Product
Thermostats > Fan Coil Thermostats > TEC3000 Series Networked and Wireless Proportional Fan Coil and Individual Zone thermostats with Dehumidification Capability
Document type
Quick Start Guide
Document revision
G
Revision date
2024-03-08
docpartnumberlabel
Part No.
Part number
24-11353-00028

Table 1 describes the touchscreen icons on the home screen. Press and release a touchscreen icon to activate the TEC. Additional touchscreen icons appear based on the menu, and those icons are also described in Table 1.

Table 1. Touchscreen icons
Icon and icon name Description

Menu

Displays the configuration screens where various settings may be adjusted.

Alarm

Indicates that the thermostat has triggered an alarm.

Unit Power

On

Standby

Powers the thermostat on or off.

Notes:

  • This icon disables all equipment control but does not physically power down the unit.
  • On the modern home screen, if the Unit Power icon is in standby mode, the temperature and humidity also display in standby mode to indicate that control off or standby mode is active.

Humidity

On

Standby

Indicates the humidity reading.

Degree

On

Standby

Indicates that the unit is set to degrees.

Network Communication (for Networked Models)

Network communication

No Signal

Network Communication icon indicates that the thermostat detected a supervisory controller and both are online.

No icon indicates that the thermostat did not detect a supervisory controller.

Radio Signal (For Wireless Models)

No signal

Low signal

Medium signal

High signal

Indicates the strength of the radio signal.

Arrow Up

Arrow Down

Increases or decreases the cooling value on the home screen.

Arrow Up

Arrow Down

Increases or decreases the heating value on the home screen.

Cooling Hold

Indicates that cooling hold mode is enabled. To disable Hold mode, press the button.

Heating Hold

Indicates that heating hold mode is enabled. To disable Hold mode, press the button.

Cooling Setpoint

Displays the current cooling setpoint. Indicates that Hold mode is disabled. To enable Hold mode, press the button.

Heating Setpoint

Displays the current heating setpoint. Indicates that Hold mode is disabled. To enable Hold mode, press the button.

Setpoint Temperature

Displays the current setpoint temperature. Indicates that the Show Hold button is set to No.

Heating Mode

Indicates that heating mode is selected.

Cooling Mode

Indicates that cooling mode is selected.

Auto Mode

Indicates that Auto mode is selected.

Fan Overrides for Single-speed Fans

On

Auto

Quiet

Adjusts the fan override between On, Auto, and Quiet for single-speed fans.

Fan Overrides for Variable-speed Fans

On

Auto

Quiet

Adjusts the fan override between On, Auto, and Quiet for variable-speed fans.

Fan Overrides for Multi-speed Fans

Low

Medium

High

Auto

Quiet

Adjusts the fan override between Low, Medium, High, Auto, and Quiet for multi-speed fans.

Occupancy Status

Unoccupied

Occupied

Temporarily occupied

Standby

Override-occupied

Override-unnoccupied

Adjusts the occupancy between Unoccupied, Occupied, Temporarily occupied, Standby, Occupancy override, Unoccupancy override.

Back

Moves the display to the previous screen.

Forward

Moves the display to the next screen.

Home

Returns the display to the main home screen.

Save

Saves the current configuration and parameter settings.

Delete

Deletes the scheduled event.

Clear

Clears the password entry on the keypad screen.

Exclamation point

Indicates that an error has occurred.