Overview - Johnson Controls - TEC312x-14-xxx - TEC3023-1x-xxx - TEC3322-1x-xxx - TEC3622-1x-xxx - TEC3022-1x-xxx - TEC3623-1x-xxx - TEC3323-1x-xxx - Proportional Fan Coil Thermostat - Thermostats - TEC3000 Series Networked and Wireless Proportional Fan Coil and Individual Zone thermostats with Dehumidification Capability

TEC3000 Series Proportional Fan Coil Thermostats Quick Start Guide

Product
Thermostats > Fan Coil Thermostats > TEC3000 Series Networked and Wireless Proportional Fan Coil and Individual Zone thermostats with Dehumidification Capability
Document type
Quick Start Guide
Document revision
G
Revision date
2024-03-08
docpartnumberlabel
Part No.
Part number
24-11353-00028

About this task

Figure 1 shows the thermostat home screen in both the light and dark themes. You can customize it to show or hide various elements from the occupant. See Table 1 for a listing of the touchscreen icons. When screen customization is used in conjunction with a passcode, the building owner can control which options the occupant can access and adjust.

Important: If lockout levels are used, some icons are hidden. Table 1 provides details of these levels.
Figure 1. thermostat home screen (shown with light and dark themes)

To switch between the modern, classic, light, and dark themes, complete the following steps:

Procedure

  1. Press the Menu icon.
  2. Press Settings.
  3. Press Display Settings.
  4. Press Change Color Theme.
  5. Select one of the four options available.

Results

Multiple pages are available on the display. The page that you currently view is emphasized with a filled dot. The other available page displays as an empty dot.

In the modern theme, the cooling, or blue, and heating, or orange, circles show whether the cooling or heating mode is active.

Figure 2. thermostat home screen in cooling mode (left) and heating mode (right)