Customizing the home screen - Johnson Controls - TEC312x-14-xxx - TEC3023-1x-xxx - TEC3322-1x-xxx - TEC3622-1x-xxx - TEC3022-1x-xxx - TEC3623-1x-xxx - TEC3323-1x-xxx - Proportional Fan Coil Thermostat - Thermostats - TEC3000 Series Networked and Wireless Proportional Fan Coil and Individual Zone thermostats with Dehumidification Capability

TEC3000 Series Proportional Fan Coil Thermostats Quick Start Guide

Product
Thermostats > Fan Coil Thermostats > TEC3000 Series Networked and Wireless Proportional Fan Coil and Individual Zone thermostats with Dehumidification Capability
Document type
Quick Start Guide
Document revision
G
Revision date
2024-03-08
docpartnumberlabel
Part No.
Part number
24-11353-00028

About this task

Customizing the Home screen settings include:
  • Brightness
  • Enable Backlight
  • Units
  • Time
  • Time Zone
  • Time Format
  • Date
  • Date Format

You can also show or hide these items on the Home screen:

  • Fan Button
  • Temperature
  • Humidity
  • Off Button
  • Hold Button
  • Setpoint
  • Alarms
  • Occupancy Status
  • Unit Status
  • Date/Time

To customize the Home screen, complete the following steps:

Procedure

  1. Press the Menu icon.
  2. Press Display Settings.
  3. Enable or disable elements of the home screen as appropriate for the building owner and occupants.
  4. Set the passcode on the thermostat to prevent the occupants from changing settings that they should not have access to change.